January 6, 2022
TDK Corporation (TSE: 6762) introduces the T5828 SoundWire™ MEMS microphone as part of the SmartSound™ family of performance products for mobile, TWS, IoT and other consumer devices. This family of high-performance microphones pushes the boundaries of microphone acoustic performance, providing advanced feature sets in small package footprints. The T5828 SoundWire™ MEMS microphone offers a high acoustic overload point (AOP) of 133dB SPL, high signal-to-noise ratio (SNR) 68dBA and wide dynamic range, ideal for environments that shift from very quiet to very loud.
The T5828 microphone:
“TDK continues to expand the SoundWire™ ecosystem by introducing T5828, the most advanced SoundWire™ MEMS microphone available today,” said Ritesh Tyagi, Vice President of Product Management at InvenSense, a TDK group company. “In partnership with Qualcomm, we are demonstrating the advantages of SoundWire™ allowing a simple two wire interface for up to eleven audio devices, a bi-directional audio data stream, and a superior control interface compared to other digital interfaces.”
The TDK T5828 has a small 3.5 × 2.65 × 0.98 mm bottom port package and is available for sampling. For additional information, please contact sales@invensense.com or visit https://invensense.tdk.com/smartsound/. TDK will be introducing the T5828 during the 2022 CES Virtual Press Conference for more information contact pr@invensense.com.
Product | Package Size | SNR (HQM / LPM) | AOP dB SPL (HQM / EAOPM) | Power µA (ULPM / LPM / HQM / ) | LFRO (Hz) | Interface |
---|---|---|---|---|---|---|
T5828 | 3.5 × 2.65 × 0.98 | 68 | 133 / 136 | 95 / 130 / 330 | 28 | SoundWire® |
TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK’s comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2021, TDK posted total sales of USD 13.3 billion and employed about 129,000 people worldwide.
InvenSense, Inc., a TDK Group company, is a world leading provider of high performance MEMS sensor platforms. InvenSense’s vision of Sensing Everything® targets the consumer electronics and industrial areas with integrated Motion, Sound, and Ultrasonic solutions. InvenSense’s solutions combine MEMS (micro electrical mechanical systems) sensors, such as accelerometers, gyroscopes, compasses, microphones, and ultrasonic 3D-sensing with proprietary algorithms and firmware that intelligently process, synthesize, and calibrate the output of sensors, maximizing performance and accuracy. InvenSense’s motion tracking, ultrasonic, audio, fingerprint, location platforms and services can be found in Mobile, Wearables, Smart Home, Industrial, Automotive, and IoT products. InvenSense became part of the MEMS Sensors Business Group within the newly formed Sensor Systems Business Company of TDK Corporation in 2017. In February of 2018, Chirp Microsystems joined the InvenSense family through its acquisition by TDK. InvenSense is headquartered in San Jose, California and has offices worldwide. For more information, go to invensense.tdk.com
You can download this text and associated images at https://invensense.tdk.com/news-media/tdk-launches-3-new-smartsound-mems-microphones-with-soundwire-functionality
Further information on the products can be found under https://www.invensense.tdk.com/technology/smartsound/